AXIS#.VL.THRESH

Description

AXIS#.VL.THRESH sets the user over-speed fault threshold. This threshold becomes the overall over-speed fault threshold (AXIS#.VL.VFTHRESH) if it is less than the motor speed threshold (1.2 x AXIS#.MOTOR.VMAX), and for AXIS#.MOTOR.TYPE = 6 if it is less than the motor back EMF overspeed threshold ((1.02 x 1000 x VBUS.OVFTHRESH) / (AXIS#.MOTOR.KE x sqrt(2))).

The value is considered an absolute value, hence it applies for both negative and positive velocities.

Example

AXIS#.VL.THRESH is set to 600 rpm. A velocity (AXIS#.VL.FB ) of 700 rpm will generate an over speed fault.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

See Velocity Units for details.

Range

Depends on units. See Velocity Range for details.

Default Value

3,600 RPM

Depends on units. See Velocity Units for details.

Data Type

Float
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
AXIS1.VL.THRESH

5011h

08h

Signed32

Velocity

-

Read/Write

No

AXIS2.VL.THRESH

5111h

08h

Signed32

Velocity

-

Read/Write

No

EtherNet/IP

Name

ID

Hex

Data Type

Access

Units

AXIS1.VL.THRESH

6034

1792

Signed32

Read/Write

Velocity

AXIS2.VL.THRESH

71570

1179

Signed32

Read/Write

Velocity

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.VL.THRESH

6034

Float

Read/Write

Velocity